WinStudio
The Import Files and Folders dialog is used to add or replace web asset global objects, including:
The system first looks for the assemblies in the forms metadata, then attempts to find them on the disk.
The Source Folder field is used to select the location of files stored on the file system. The Target Path field indicates the root path to use for imported files. The effective path for an imported file is constructed by adding the Target Path to the Source Folder.
Click the Source Folder button to select a new folder.
Click the Add Files button to select files and folders to import. Selecting a folder selects all files within the folder.
Creating a User Control and a User Control Component