A WinStudio menu that is specific to a particular IDO collection on a form. The menu is always the second menu on the menu bar when a form is open. The displayed name of the menu is specified in Configuration Manager. By default, the name is "Actions." The name can be set to a literal or string value such as "Objects," which displays when any form is open; or the name can be set so that it changes dynamically to match the caption of the current form. The shortcut menu that opens when a user right-clicks a form contains the same commands as the Actions menu.