WinStudio
Use this dialog box to add, configure, and delete components within a container component. This dialog box is accessed by clicking the Edit button in the upper left corner of any container component while in Design Mode.
Container components include:
This dialog box consists of two basic sections:
For example, if this dialog box is accessed from a grid, the list displays, in order, all the columns currently defined for the grid.
| Control | Description/Comments |
Delete button |
Deletes the selected component from the list |
Move Up button |
Moves the selected component up in the list |
Move Down button |
Moves the selected component down in the list |
Copy/Paste button |
Copies the selected component to a selected container This button opens the Select Container for Pasted Component dialog box, which allows you to specify where and how the copied component is to be pasted. |
Container component display |
(Read-only) Displays the name of the container to which the contained components are assigned If there are multiple containers, you can select the one you want from the drop-down list. |
Add button |
Adds a contained component to the list |
These sheets are identical to their counterparts in the main WinStudio Design Mode property sheet displays. Once the contained component exists, you can configure it in either place and the results are the same.
Setting Form, Component, and Object Properties
About Notebook and Notebook Tab Components
About Grid and Grid Column Components
About Vertical Grid and Vertical Grid Element Components