WinStudio
Edit Validators Dialog Box
Use this dialog box to specify one or more validators for a component.
Validators for a component are executed in the order they appear in the
list in this dialog box.
- To create a new validator for a component, click the New icon.
The system adds the new validator to the application's validator set
and makes it available to other components.
- To add an existing validator to the list for a component, click
the Add icon.
- To edit a validator, select the validator from the list and click
the Edit icon.
CAUTION:
Be careful when editing validators, especially if you are editing a validator
that might be used with other components. Editing a validator for one
component affects any other component that uses that same validator.
- To remove a validator from use with a component, select the validator
in the list and click the Delete icon.
NOTE:
Removing a validator here does not delete the validator from the
system. It still exists and can be used with other components. To delete
the validator from the system, you must use the Validators dialog box.
- To specify substitution strings for the system to use for parameters
during the execution of the validator, click the Parms (Parameters)
icon. This opens the Edit Validator
Sub Parms dialog box. To implement these substitution
strings, you must specify corresponding parameters in the Inheritance > Parameters
property field for the component.
- To change the sequence of validators in the list (which affects
the order in which they execute), use the Up and Down arrow icons.
When you are finished with your validator specifications, click OK.
Related Topics
Create,
Copy, Edit, or Delete Validators
Maximum
Length of Parameters and Values
Tip:
Choosing Efficient Validators
Tip:
Reducing Round Trips to the Server
Tip:
Using List Sources and Validators
Understanding
Validators
Validator
Types