WinStudio
Edit Action Dialog Box
Use this dialog box to specify the "action" part of a
conditional action value expression for a component.
| Action Type |
Specify the type of conditional action to define:
- NONE - Nothing happens. This setting is the default
when you create a new conditional action.
- Set - Sets a value for the component if the condition
evaluates to true.
- SetModified - Sets a value for the component and marks
the record as modified, if the condition evaluates to
true.
- Enabled - Enable the component if the condition evaluates
to true, or disable the component if the condition evaluates
to false.
- Required - Make the component a required field if the
condition evaluates to true.
- Visible - Make the component visible if the condition
evaluates to true, or hide the component if the condition
evaluates to false.
- Toggle - Turn the component setting on or off based
on the condition setting.
- Modified - Mark the record as modified if the condition
evaluates to true.
- GenEvent - Generate an event if the condition evaluates
to true.
- GenEventRet - Generate an event and return a value
if the condition evaluates to true.
- Focus - Sets focus on the component if the condition
evaluates to true. If the condition evaluates to false,
focus on another component, if supplied in the expression.
- ReturnValue - Sets the return value based on the conditional
action.
- Stop - If the condition evaluates to true, stop execution
of any additional actions on the overall expression.
- Validate - If the condition evaluates to false, display
the message specified in the expression.
See Conditional
Action Syntax for details about the actions. |
| Action Value |
Enter a value or click Edit Value to display the
Edit
Value Expression dialog box. |
Related Topics
Creating
a Conditional Action Expression - Simple Example
Conditional
Action Syntax
Enabled When, WinStudio
Component Property
Required When, WinStudio
Component Property
Visible When, WinStudio
Component Property