WinStudio
Use this dialog to specify a condition to include in a conditional action expression for a component.
| Up | Move the selected condition clause up in the order. |
| New | Creates a new row (clause) in the condition. |
| Delete | Delete the selected clause. |
| Down | Move the selected clause down in the order. |
| Left Value | This field displays the value set for the left side of the current clause in the conditional expression. Click Edit Left Value to open the Edit Value Expression dialog box and specify a different Value Type or Value for the current clause. |
| Operator | Specify the operator used to compare the Left Value with the Right Value. |
| Right Value | This field displays the value set for the side side of the current clause in the conditional expression. Click Edit Right Value to open the Edit Value Expression dialog box and specify a different Value Type or Value for the current clause. |
| And With Next Clause | You can create multiple clauses and join them by a Boolean AND filters. Clauses joined by AND allow for only those conditions that meet the criteria specified in all clauses. If you do not select this check box, the clause is defined as an OR clause. Clauses joined by OR allow for conditions that meet any one of the criteria specified in the clauses. |
Creating a Conditional Action Expression - Simple Example
Enabled When, WinStudio Component Property
Required When, WinStudio Component Property
Visible When, WinStudio Component Property