WinStudio

Edit Drag From/Drop On Events Dialog Box

Use this dialog box to make "Drag From" and "Drop On" event assignments.

NOTE: The exact name of this dialog box depends on the context from which it is called: If it is being opened to assign "Drag From" events, it is labeled the Edit Drag From Events dialog box. If it is being opened to assign "Drop On" events, it is labeled the Edit Drop On Events dialog box. In both cases, however, the functionality is the same.

Adding an Event

To add an event to be generated during drag-and-drop operations:

  1. In the Event to Add field, specify the name of the event to be generated. You can either:
  2. Click Add.
  3. The names of all events specified for this operation display in the list field.

  4. Click OK.

Deleting an Event

To delete an event from the list, so that it is no longer generated during drag-and-drop operations:

  1. In the list of events currently assigned, select the event to delete.
  2. Click Delete.
  3. The event no longer displays in the list.

  4. Click OK.

Related Topics

About Drag and Drop in Forms

Using Drag-and-Drop in Forms

Drag From Events Property

Drop On Events Property

Drag Image Property