WinStudio
Use this dialog box to specify the parameters required by an IDO method call. You can specify a literal, property, variable, or component value as a parameter. Method call validators can also output values to properties, variables, or components.
| Type | The type of parameter required by the IDO method. The options
are:
Variant |
| Output | Select this check box if a method call validator outputs values to a property, variable, or component. Otherwise, clear this check box. |
| Value Type | The type of value required by the parameter of the IDO method. You can specify a literal, property, variable, or component value as a parameter. |
| Value | Depending on the Value Type, enter a literal value or select a property, variable, or component that supplies the value. |
| Edit Target | If the Value Type is Variable or Component, click this button to edit the variable or component referenced. |
Create, Copy, Edit, or Delete Validators
Maximum Length of Parameters and Values
Tip: Choosing Efficient Validators
Tip: Reducing Round Trips to the Server
Tip: Using List Sources and Validators