WinStudio
For In Collection, In Inline List, In List Cache, Method Call, and Set From List Only validators, use this dialog box to output values to properties, variables, and components.
This dialog box provides these options:
| Field/Button/Option | Description/Comments |
Variables |
The button launches the Edit Set Variable Values dialog box, from which you can add, modify, rearrange, or delete variables and their corresponding values. The field displays the variables and the values they are to be set to. These variable/value pairs must use the syntax variable=value. |
Components |
The button launches the Edit Set Component Values dialog box, from which you can add, modify, rearrange, or delete components and their corresponding values. The field displays the components and the values they are to be set to. These component-value pairs must use the syntax component=value. |
Properties |
The button launches the Edit Set Property Values dialog box, from which you can add, modify, rearrange, or delete properties and their corresponding values. The field displays the properties and the values they are to be set to. These property-value pairs must use the syntax property=value. |
Do not mark output targets modified? |
When selected, this option invokes the NOMOD keyword, which instructs WinStudio to NOT mark the output target values as modified. This is required for cases where you do not want the values of the target components or properties to be revalidated after the event handler executes. NOTE: This option is not available when this dialog box is launched from the Edit In Collection Validator Parameters or Edit Inline List Validator Parameters dialog box, because, in those case, the policy for marking output targets is modified from those dialog boxes. |