WinStudio
Use this dialog box to set up and maintain the specifications for an event handler with the Generate Event response type.
Event |
The name of the standard event or custom event to be generated by the event handler. |
Post event asynchronously |
To have the system generate the event handler after the current processing is completed, select this field. |
About Generating Events from Components
Create, Copy, Edit or Delete Event Handlers
Event Handler Response Types (WinStudio)
Maximum Length of Parameters and Values
Understanding the WinStudio Event Model