WinStudio
Use this dialog box to create a new script or to copy a script with a new name. When you click OK, WinStudio opens your designated scripting editor and displays the script you specified.
Script Name |
Specifies the name of the new script you are creating or the name of the script to which you are copying a selected script. |
Language |
Specifies the scripting language to be used for the script. Options are:
NOTE: If the Allow script language selection option on the Process Defaults forms is set to 0, this option is disabled. |
About IDOCollection Object (WinStudio Scripts)
About FormComponent Object (WinStudio Scripts)
About Form Object (WinStudio Scripts)
About WinStudio Application Object (WinStudio Scripts)
Create, Copy, Edit, or Delete Global Scripts
Maximum Length of Parameters and Values
Referencing Variables in WinStudio Scripts
Understanding Scripts in WinStudio