WinStudio

Specify Chart Settings Dialog Box

Use this dialog box to specify settings for a chart component. Not all settings are required; if you do not specify a value for an optional setting, a default value is used.

As used in this topic:

Data Tab

This tab specifies general information about the type of chart, as well as the data binding.

Chart Attributes

Field Description
Chart Style Specify the style of chart:
  • Single Series Charts depict one set of data, for example one month.
  • Multi Series Charts depict one or more sets of data, for example multiple months.
  • Combination Charts combine two or more chart types, for example a bar and a line chart.
Chart Type The list of chart types depends on the Chart Style you selected:
  • Single Series Charts include: Column2D, Column 3D, Line, Area 2D, Bar 2D, Pie 2D, Pie 3D, Doughnut 2D, Doughnut 3D, Pareto 2D, Pareto 3D, Spline, SplineArea, Waterfall2D, Funnel, Pyramid, SparkLine, and SparkColumn.
  • Multi Series Charts include: MSColumn2D, MSColumn3D, MsLine, MSBar2D, MSBar3D, MSArea, Marimekko, ZoomLine, ScrollColumn2D, ScrollLine2D, ScrollArea2D, StackedColumn2D, StackedColumn3D, StackedBar2D, StackedBar3D, StackedArea2D, MSSpline, MSSplineArea, LogMSColumn2D, LogMSLine, InverseMSArea, InverseMSColumn2D, InverseMSLine, Radar, and MSStepline.
  • Combination Charts include: MSCombi2D, MSCombi3D, and MSColumnLine3D.

To see an example of each chart type, select the chart type and click Preview.

Caption Specify the caption (title) for the chart.

Note: You can set the font, color, and size of the text for the chart on the Other tab.

Sub-Caption Specify the subtitle, if any, for the chart.
X-Axis Name Specify the label for the X (horizontal) axis.
Y-Axis Name Specify the label for the Y (vertical) axis.

Axes

Field Description
Property for X-Axis Labels Select the property from the collection to use for the X-axis labels.

Binding

Field Description
Bind Chart to Entire Collection Use this option to chart all the data in the collection together.   For example, this option is useful on mobile forms.
Bind Chart to Current Row Use this option if you want the chart data to change on selection of each row. This option will be used on most Multiview forms

Chart Data

Field Description
Collection Specify the collection whose properties you want to chart. The drop-down list includes all IDO collections that are available on the current form.
Available Properties Select a property from the collection and click Add>> to add it to the list of fields you want to chart. For example, you might want to chart quantities and amounts on a form. To remove a property from the list of fields you want to chart, click <<Remove.  Use the Up and Down buttons to move properties within the list.

These properties represent the series of the chart, so for a multi-series chart, you specify multiple properties here. If you specify multiple properties for a single-series chart, only the first property is used; the others are ignored.

Render As Specify how each series of a combination chart is rendered: as a Column, Area, or Line. For example, if you specify MSCombi2D as the chart type, and you then add two series to the property list and set Render As to Line for one of the properties, one series is displayed as a column chart and the other series is displayed as a line chart.

Trend Lines Tab

Trend lines are horizontal or vertical lines that help users interpret the data in relationship to a predetermined value. For example, a trend line can indicate the target values.

Field Description
Start and End Values If you are defining a  trend line, specify just a starting value.  If you are defining a slanted trend line, specify starting and ending values. If the value you specify is not within the chart limits, the trend line or zone is not included.
Display Value Specify the label, if any, for the trend line.
Color Double-click to display the Color dialog box, where you can select a color or define a custom color for the trend line.  The color is displayed in hexadecimal after you apply your changes.
Trend Zone Select to mark a trend zone (range of values) instead of a line.
Show On Top Select to display the trend line or zone on top of the chart values.
Thickness Specify the thickness of the line, in pixels.
Alpha Specify the transparency of the trend line, from 0 to 100.
Dashed

Dash Length

Dash Gap

Select Dashed to use a dashed line. You can also specify the length of the dash and the gap between dashes, in pixels.
Value on Right Select to show the trend line label to the right of the chart.
Tool Text Specify the tool text, if any, that displays when you hover over the line.

General Tab

Legend

In multi-series or combination charts, the name of each dataset is displayed in the legend of the chart, to link data to its description by color. The legend is not displayed for single-series charts.

Field Description
Show Legend Select to display the legend for the chart.
Legend Caption Specify the caption to use for the legend.
Legend Position Specify BOTTOM or RIGHT to indicate where the legend is displayed.
Back Color Double-click to display the Color dialog box, where you can select a color or define a custom color for the background.  The color is displayed in hexadecimal after you apply your changes.

To use a gradient fill, specify each of the colors required for the gradient fill as hexadecimal, separated by commas.

Back Alpha Specify the transparency of the background, from 0 to 100.
Border Color Double-click to display the Color dialog box, where you can select a color or define a custom color for the canvas border.
Border Thickness Specify the thickness of the border around the legend (in pixels).
Border Alpha Specify the transparency of the legend border, from 0 to 100.
Show Legend Shadow Select to display a shadow for the legend.
Reverse Legend Select to reverse the order of the items in the legend. This can be useful in stacked charts.

Functional Attributes

Field Description
Palette Specify a palette number, from 1 to 5, with 1 as the default. You can select a palette and click Preview to see what it looks like. The palette theme configures colors for:
  • Background and border
  • Canvas border and background
  • Fonts
  • Div lines
  • Tooltip
  • Anchors
  • Legend
Palette Colors To specify custom colors for a palette, instead of using one of the predefined themes, specify the colors in hex, separated by commas.
Label Display Specify how you want long X-Axis labels to be displayed:
  • AUTO: Automatically use the best display mode (rotate or wrap).
  • WRAP: Wrap labels in multiple lines. If there is not enough space, labels are automatically trimmed, with ellipses (...) added and tool-tips displayed on mouseover.
  • STAGGER: Distribute labels along multiple lines under the chart.
  • ROTATE: Rotate labels so they display vertically.
  • NONE: Do not display labels.
Label Step If X-axis labels represent an incremental quantity such as dates, specify a number (n) here, to display every n-th label instead of all labels. This can make a chart less cluttered.
Y-Axis Values Step If Y-axis values represent an incremental quantity with divisional lines or grids, specify a number (n) here, to display a value on every n-th line.  Specify 1 or leave blank to display a value on every line.
Y-Axis Min Value Specify the minimum value to display on the Y-axis. Otherwise, the system determines the value automatically based on the available data.
Y-Axis Max Value Specify the maximum value to display on the Y-axis. Otherwise, the system determines the value automatically based on the available data.

For example, a percent chart normally ranges from 0 to 100. If your allowable data range is only from 1 to 10, you can use those values as the min and max.

Animated Select to animate the chart so that data displays gradually, rather than all at once.
Show/Rotate/Slant Labels Specify whether you want to display X-axis labels on the chart, and if so, whether they should be rotated (displayed vertically) or slanted at 45 degrees.
Show/Rotate Values Specify whether you want to display data values on the chart, and if so, whether they should be rotated (displayed vertically).
Place Values Inside Select to display data values inside the chart objects that represent them.
Show Y-Axis Values Select  to display Y-axis data values on the chart.
Show Limits Select to display the Y-axis upper & lower limit values on the chart.
Show Div Line Values Select to display values for divisional lines, which are horizontal lines that divide the Y-axis into smaller units.
Show Shadow Select to add a shadow effect to the chart.
Auto Div Line Adjust Select to automatically set the Y-axis upper & lower limit values and the number of divisional lines.
Rotate/Center Y-Axis Name Select this option to display the Y-Axis name vertically. Clear this option to show the name horizontally and centered.

Cosmetics Tab

Padding and Margins

Padding and margins are specified in pixels.

Field Description
Caption Padding Specify the space between the chart caption and the top of the chart canvas. If a subcaption is defined, this value controls the space between the subcaption and the top of the canvas.
X-Axis Name Padding Specify the distance between the top of the X-Axis title and the bottom of data labels (or canvas, if data labels are not displayed).
Y-Axis Name Padding Specify the distance between the Y-Axis name and values.
Y-Axis Values Padding Specify the padding between the left side of the chart canvas and the Y-Axis values.
Label Padding Specify the vertical space between the bottom of the canvas and the data labels.
Value Padding Specify the space between the columns or anchors and the value text boxes.
Plot Space Percent On a bar or column chart, define the spacing between bars or columns, from 0 to 80. By default, the spacing is set to 20% of canvas width. For example, if you want bars flush against each other, set this value to 0. If you want thin bars with a lot of space between, set this value to 80.
Margins Chart margins are the padding between the chart border and the canvas. Each of the margins - left, right, top, and bottom - can be set individually.
Canvas Margins Canvas margins are the padding between the start of the chart canvas and the chart itself. Each of the margins - left, right, top, and bottom - can be set individually.

For 2D charts, the canvas is the visible rectangular box. For 3D charts, the canvas is the imaginary box around the 3D canvas.

By default, the system calculates the margin space based on the elements placed on the chart. Use this attribute to override the default space with a higher value. You cannot specify a lower value. This attribute is helpful if you have multiple charts on a page and you want all of the canvases to align with each other.

Cosmetics

Field Description
Back Color/Alpha/

Ratio/Angle

Color: Double-click to display the Color dialog box, where you can select a color or define a custom color for the chart background.  The color is displayed in hexadecimal after you apply your changes. To use a gradient fill, specify all the colors required for the gradient fill, separated by commas.

Alpha: For each color you specified above, specify the transparency of the background, from 0 to 100. Separate the alphas by commas.

Ratio: Specify the ratio of each color in the gradient on a scale of 100. The total of the ratios must equal 100. For example, to plot an equidistant gradient for two colors, specify the ratio as 0,100.

Angle: Specify the angle of the gradient fill, in degrees, from 0 to 360.

Show Border Select to display an outer border around the whole chart, containing the canvas and the legend as well.
Border Color/ Thickness/Alpha Color: Double-click to display the Color dialog box, where you can select a color or define a custom color for the border around the chart. The color is displayed in hexadecimal after you apply your changes.

Thickness: Specify the thickness of the border, in pixels.

Alpha: Specify the transparency of the border.

Canvas Back Color/Alpha/ Ratio/Angle Color: Double-click to display the Color dialog box, where you can select a color or define a custom color for the canvas background.  The color is displayed in hexadecimal after you apply your changes. To use a gradient fill, specify all the colors required for the gradient fill, separated by commas.  

Alpha: For each color you specified above, specify the transparency of the background, from 0 to 100. Separate the alphas by commas.

Ratio: Specify the ratio of each color in the gradient on a scale of 100. The total of the ratios must equal 100. For example, to plot an equidistant gradient for two colors, specify the ratio as 0,100.

Angle: Specify the angle of the gradient fill, in degrees, from 0 to 360.

Canvas Border Color/Thickness/ Alpha Color: Double-click to display the Color dialog box, where you can select a color or define a custom color for the border around the canvas.  The color is displayed in hexadecimal after you apply your changes.

Thickness: Specify the thickness of the border, in pixels.

Alpha: Specify the transparency of the border.

Note: There is a Show Border property to show or hide the outer border, but there is no Show Canvas Border property to show or hide the canvas border. However, you can still hide the canvas border by setting its Alpha value to 0.

Show V-Line Label Border Select to display a border for the V-Line label. The V-Line is a vertical, or horizontal in the case of bar charts, separator line used to separate blocks of data.  

Data Plot Cosmetics

Field Description
Use Round Edges Select to plot chart objects with round edges and fill them with a glass effect gradient. When you select this option, plot fill and borders are not displayed.
Show Plot Border Select to display borders on the plotted chart objects.
Plot Border Color/Thickness/ Alpha Specify the plotted chart objects' border color (double-click to select), thickness (from 0 to 5 pixels), and alpha gradient (from 0 to 100).
Plot Border Dashed/ Dash Length/Gap Select Dashed to use a dashed line for the plot border. You can also specify the length of the dash and the gap between dashes, in pixels.
Plot Fill Angle/Ratio/Alpha If you chose to fill the plot object with a gradient, specify the fill angle for gradient (0 to 360), the ratio for the gradient (0 to 100), and the alpha (0 to 100).
Plot Gradient Color Double-click to select a second color to globally add a gradient to the entire plot of the chart. For example, if you specified individual colors for columns, to create a gradient that ends in white, specify FFFFFF (white) here, and the chart draws plots as gradient.

Anchors

Anchors, or marker points, are polygons that are displayed where two consecutive lines or area points are joined on a line or area chart. These indicators show the position of data points. The anchors can be used to display tool tips and links for the data points. If anchors are hidden, tool tips are not displayed and links will not work.

Field Description
Draw Anchors Select to display anchors on the chart.
Anchor Side/ Radius Side: Specify the number of sides, from 3 to 20, that the anchor has. For example, an anchor with 3 sides is displayed as a triangle.

Radius: Specify the radius, in pixels, of the anchor. A larger radius draws a larger anchor.

Border Color/ Thickness Color: Double-click to display the Color dialog box, where you can select a color or define a custom color for the border around the anchor.  The color is displayed in hexadecimal after you apply your changes.

Thickness: Specify the thickness of the border, in pixels.  

Back Color Double-click to display the Color dialog box, where you can select a color or define a custom background color for the anchor.  The color is displayed in hexadecimal after you apply your changes.
Alpha Specify the transparency of the anchor, from 0 to 100.
Back Alpha Specify the transparency of the anchor background, from 0 to 100.

Other Tab

Font

Field Description
Base Font/Size/ Color Specify the font to use for all text on the chart. Specify a font size (0 to 72) and double-click in the Color field to select a font color.  If you also specify an outside canvas font, the base font applies only to tooltips and data values.
Outside Canvas Font/Size/Color If you specify a second font for the outside canvas, that font applies to all text that lies outside the canvas. Specify a font size (0 to 72) and double-click in the Color field to select a font color.

Tooltips

Field Description
Show Tooltip Select to display tool tips when the mouse hovers over a data point. Tool tip information depends on the type of chart:
  • For single series charts except pie and doughnut: Name and value
  • For pie and doughnut charts: Name and value/percentage
  • For multi-series and combination charts: Series name, category name, and data value
Show Tooltip Shadow Select to display a shadow on tool tips.
Series Name in Tooltip Select to include the series names (X-axis labels for data points) in the tool tip.
Tooltip Back Color Double-click to select a background color for the tool tip.
Tooltip Border Color Double-click to select a border color for the tool tip.
Tooltip Separator Char Specify a separator character to use between different types of information in the tool tip.

Number Formatting

Field Description
Format Number Select to automatically add commas to numbers in the appropriate places.
Format Number Scale Select to automatically format numbers by adding K (kilo, for thousands) or M (million) and truncating the numbers. For example, 10,000 is truncated to 10K.
Force Decimals Select to include trailing zeros if necessary so that all values in the chart are displayed to the decimal precision specified in Decimal Places, below.
Force Y-Axis Decimals Select to include trailing zeros on the secondary axis on dual Y-axis charts, if necessary, so that values in the secondary axis are displayed to the decimal precision specified in Y-Axis Decimal Places, below.
Default Number Scale and Unit/ Value Use the number scale and number scale unit/value together to define units of scaling for the chart. By default, the charts use (1000,1000) (K,M) scaling, which equates to 1000 = 1K and 1000K = 1M.  To add billions to the scaling, set the Scale to 1000,1000,1000 and the Unit/Value to K,M,B, which equates to 1000=1K, 1000K=1M, and 1000M = 1B.  To use a time scale, set the Scale to 60,60,24,7 and the Unit/Value to min,hr,day,wk, which equates to 60 seconds = 1 min, 60 minute = 1 hr, 24 hrs = 1 day,
and 7 days = 1 week.
Number Prefix/Suffix Prefix: Specify a value to add it as a prefix to all numbers plotted on the primary axis. For example, to display all numbers as dollars, specify  $ as the prefix.

Suffix: Specify a value to add it as a suffix to all numbers plotted on the primary axis. For example, to display all numbers as per year, specify /yr as the suffix.

Decimal Separator Specify a decimal separator if you do not want to use the default value, which is a period.
Thousand Separator Specify a thousands separator if you do not want to use the default value, which is a comma.
Decimal Places Specify the number of decimal places to round to.  This controls the decimal precision of all numbers on the chart. For example, if your data includes 0.12352, 0.134 and 0.13, and you set this value to 3, the data is displayed as 0.124, 0.134 and 0.13. Note that the system does not add the 0 padding to 0.13 to form 0.130.  To force the display of trailing zeros, use Force Decimals (above).
Y-Axis Decimal Places On dual Y-axis charts, specify the number of decimal places to round to, for the secondary Y-axis. To force the display of trailing zeros, use Force Y-Axis Decimals (above).

Divisional Lines

Divisional lines are horizontal lines running through the canvas, dividing the y-axis into smaller units.

Field Description
Num Div Lines Specify the number of divisional lines, if you do not want to use the default value.
Div Line Color/ Thickness/Alpha Color: Double-click to display the Color dialog box, where you can select a color or define a custom color for the divisional lines.  The color is displayed in hexadecimal after you apply your changes.

Thickness: Specify the thickness of the lines, in pixels.

Alpha: Specify the transparency of the lines.

Div Line is Dashed/Dash Length/Gap Select Dashed to use a dashed divisional line. You can also specify the length of the dash and the gap between dashes, in pixels.
Zero Plane Color/Thickness/ Alpha The zero plane separates positive and negative numbers on a chart.

Color: Double-click to display the Color dialog box, where you can select a color or define a custom color for the zero plane.  The color is displayed in hexadecimal after you apply your changes.

Thickness: Specify the thickness of the plane, in pixels.

Alpha: Specify the transparency of the plane.

Show Alternate H-Grid Color/Color/

Alpha

Select Show Alternate H-Grid Color to display alternating horizontal grid bands in the color you select, with the transparency (alpha) you select.
Show Alternate V-Grid Color/Color/ Alpha Select Show Alternate H-Grid Color to display alternating vertical grid bands in the color you select, with the transparency (alpha) you select.

Chart XML Tab

This tab displays the XML that is used to generate the chart in the form. The XML is display-only.

Buttons

Click Apply to save your changes.

Click Preview to preview the chart using the options that you selected.  The previewed example does not show Framework data.

 


Related Topics

Adding Charts or Gauges to a Form