WinStudio

About Graph Components

Note: This topic applies to the graphing tool, which is supported for backward compatibility.  We recommend that, if you want to add charts or gauges to a form, use the newer FusionCharts tool instead. For more information, see Adding Charts or Gauges to a Form.

A graph component is bound to a collection and renders a business graph of the data contained in the collection. The graph component can be displayed automatically when the collection is retrieved. Changes to the collection update the graph automatically, and selecting elements in the graph navigate the collection.

Graph components have a variety of styles, including line graphs, bar graphs, pie charts and others.

A graph component is bound to a collection using the Graph Element binding type.


Related Topics

Adding Button or Edit Components to Graph Components

Adding a Graph Component