WinStudio
Alpha validators test whether the value entered is an alphabetic character. Any text with non-alphabetic characters are rejected, including numerals. You can use the following attributes to further qualify the validation:
Attribute |
Description |
|---|---|
> |
The component's value must be greater than the specified value. |
< |
The component's value must be less than the specified value. |
>= |
The component's value must be greater than or equal to the specified value. |
<= |
The component's value must be less than or equal to the specified value. |
= |
The component's value must be equal to the specified value. |
<> |
The component's value must not be equal to the specified value. |
DBCS |
Specify the double-byte character set allowed for this
entry. By default, none is specified so WinStudio does not
check for character sets. Double-byte. Any double-byte character set. Hiragana. Double-byte Hiragana only. Katakana. Double-byte Katakana only. SbKatakana. Single-byte Katakana only. Singlebyte. Any single-byte characters. |