WinStudio
Alphanumeric validators test whether the value entered is an alphabetic character or a numeral. Any text with other types of characters is rejected. You can use the following attributes to further qualify the validation:
Attribute |
Description |
|---|---|
> |
The component's value must be greater than the specified value. |
< |
The component's value must be less than the specified value. |
>= |
The component's value must be greater than or equal to the specified value. |
<= |
The component's value must be less than or equal to the specified value. |
= |
The component's value must be equal to the specified value. |
<> |
The component's value must not be equal to the specified value. |
Minimum |
For numeric values only. The same as >=. |
DBCS |
The double-byte character set allowed for this entry. By
default, none is specified so WinStudio does not check for
character sets. Double-byte. Any double-byte character set. Hiragana. Double-byte Hiragana only. Katakana. Double-byte Katakana only. SbKatakana. Single-byte Katakana only. Single-byte. Any single-byte characters. |