WinStudio

Copying/Pasting a Component

You can use the clipboard to copy and paste components on the same form or between forms. A component is pasted into the same relative position that it occupied in the original container or form.

To copy and paste a component:

  1. Open a form and enter Design Mode.
  2. If you are pasting into another form, open the destination form and enter Design Mode.
  3. On the first form, select one or more components to copy.
  4. On the Edit menu, click Copy.
  5. On the destination form, click Paste on the Edit menu.
  6. If the destination form has containers, you are prompted to identify which container is the destination for the pasted component.
  7. If necessary, reposition the pasted components.

Related Topics

Add a Component to a Form

Cut/Paste a Component

Delete a Component

Edit a Component

Enter and Exit Design Mode

Move a Component

Move or Resize with Snap-to-Grid

Save, Cancel, or Undo Changes in Design Mode

Select and Deselect Components

Type, WinStudio Component Property