WinStudio
Currency validators test whether the component's value has a valid currency format according to local settings. This validation is performed automatically for all components with a base data type of currency.
Attribute |
Description |
|---|---|
> |
The component's value must be greater than the specified value. |
< |
The component's value must be less than the specified value. |
>= |
The component's value must be greater than or equal to the specified value. |
<= |
The component's value must be less than or equal to the specified value. |
= |
The component's value must be equal to the specified value. |
<> |
The component's value must not be equal to the specified value. |
Minimum |
The same as >=. |
Maximum |
The same as <=. |