WinStudio
Inline Script validators allow you to enter the text of a short validation script directly in the Parameters row of the Validator Properties dialog box. Use an Inline Script if the entered script (including parameters) is less than 12 lines (750 characters).
If a script exceeds the maximum length, use the Run Script response type, which accesses WinStudio objects and data through the scripting API. For more information, see Related Topics.
To pass the validation, the script must return zero. If the script returns a nonzero value, WinStudio fails the validation.
About IDOCollection Object (WinStudio Scripts)
About FormComponent Object (WinStudio Scripts)
About Form Object (WinStudio Scripts)
About WinStudio Application Object (WinStudio Scripts)
Create, Copy, Edit, or Delete Global Scripts
Maximum Length of Parameters and Values
Referencing Variables in WinStudio Scripts
Understanding Scripts in WinStudio