WinStudio
Event handlers of the type Add entry to the Audit Log.
Property: Event handler parameters.
Contains a text message that, together with an existing audit log message, is inserted as an entry in the audit log when an event handler executes.
AUDITMESSAGE( description )
Part |
Description |
| description | Expression that evaluates to a string. |
You view the audit log in the Audit Log form. Audit log entries consist of four parts: log description, message type, message description, and user name. The AUDITMESSAGE keyword provides a text message specific to your event handler. The message type and message description of a log entry are parts of a stored, global message.
The following event handler parameter inserts the text "Form closed" in the Log Desc field of the audit log when the event fires:
AUDITTYPE(3) AUDITMESSAGE(Form closed)