WinStudio
Validators that perform structured output, with validator types In Collection, In List Cache, and Method Call.
Property: Validator parameters.
Marks a validator's output as validated.
MOV( )
When the MOV keyword (Mark Output Validated) is enabled for a validator, a component that has received the output from the validator is marked as validated. If the user subsequently selects Save or tabs from the component, the component's validators do not execute. A target component that is required and receives a Null value is left as modified. A component can be a target of validator output if it, or the property to which it is bound, is an output parameter on a Method Call validator or is the target in a SETPROPERTIES or SETCOMPONENTS specification.
The following parameters apply to a Method Call validator:
Acme.ResourceDefinitions.ResourceIdValid( PARMS(VAR P(%1), RVAR P(%2), MESSAGE) OIO() MOV() )