WinStudio
Data sources for forms.
Component list sources of the type IDO Collection.
Validators of the type In Collection.
Data binding for tree components.
Sets the isolation level for transactions when loading a collection, permitting or preventing dirty reads.
READMODE(COMMITTED | UNCOMMITTED)
Part |
Description |
| COMMITTED | Specifies that shared locks are held while data is being read to avoid dirty reads. The setting corresponds to the Transact-SQL statement SET TRANSACTION ISOLATION LEVEL READ COMMITTED. |
| UNCOMMITTED | Implements dirty reads, in which no shared locks are issued and no exclusive locks are honored. The setting corresponds to the Transact-SQL statement SET TRANSACTION ISOLATION LEVEL READ UNCOMMITTED. |
The READMODE setting overrides the default value for Collection Read Mode specified in the core form Process Defaults. If the keyword is not used in a collection specification, the IDO returns collections using the default value. The override applies only to the object for which it is specified.