WinStudio
Event handlers of the type Run Background Task, where the executable type is RPT (report).
Property: Validator parameter.
Passes parameters for a report's stored procedures to Task Manager.
SP( parameter1 [, parameter2, . . . ] )
Part |
Description |
| parametern | Parameters for a report's stored procedures, separated by commas. |
The executable type RPT (report) is specified in the system-support form Background Task Definitions. The SP keyword is required with Crystal Reports version 6.0 and earlier to distinguish stored procedure parameters from report parameters. See also the RP keyword.
In the following event handler parameter, the RP keyword and the SP keyword distinguish report parameters from stored procedure parameters.
TASKNAME(DISTRPT)TASKPARMS(RP(V(BeginDate), V(EndDate)) SP(V(BeginDate), V(EndDate)))