WinStudio

SUM Keyword

Applies To

Form components.

Component property: Data binding.

Description

Evaluates to the numeric sum of the values of a property in a collection.

Syntax

SUM( PROPERTY( PropertyName ) )

Part

Description

PropertyName Expression that evaluates to a string representing the name of a property of the IDO that returns the collection.

Remarks

A substitution keyword. Use the SUM keyword to specify the data binding of a read-only component. The sum is updated when the StdFormLoadDerivedValues event is generated during, for example, a Save or navigate operation. To force an update when the value of the property changes, use the DEPENDENCY keyword with the SUM keyword.

Example

The following example is a data binding specification for a read-only edit text box. The value of the component is the sum of the property values in the QuantityShipped column of a collection.

SUM(PROPERTY(QuantityShipped))