WinStudio
Use the Bitmap File Name property to specify the name of a graphic file to display in a component. You can display graphics in static components that have no data binding and in button components.
Supported formats:
Binary Data Format | Default Extension |
---|---|
BMP | bmp |
EMF | emf |
EXIF | exif |
GIF | gif |
ICON | ico |
JPEG | jpg |
PNG | png |
TIFF | tif |
WMF | wmf |
You can select an image file located in the main program folder (the folder in which WinStudio.exe is located) or browse other folders. To locate a file in the main program folder, select a file name from the drop-down list. To browse other folders, click the browse button.
It is recommended that you specify a file located in the main program folder and distribute the file to users in that folder. If you specify a path as well as a file name, the path must be valid on each WinStudio client. For Web rendering, these files must also be placed in the WSWebClient\Content\images folder.