WinStudio

Find Form Property

Use the Find Form property to specify the name of a query form that is opened when the user selects Find from a component's shortcut menu.

The Find menu command is a data drill-down feature. To enable the feature, you must specify a shortcut menu for a component in its Right-Click Menu property.

The command opens the query form associated with the form used to maintain the object referenced in the current component. The user can select an object in the query form. The object can be returned to the component.

An order-entry form, for instance, typically contains a Customer ID component that is used to reference the customer placing the order. Detailed information about the customer is typically maintained in a separate Customers form. The Find command on the shortcut menu for the Customer ID component can be set to open the query form associated with the Customers form.

To specify additional criteria for opening the query form, click the ellipsis (...) button.


Related Topics

About Query Forms

Add/Details Form, WinStudio Component Property

Create a Query Form

Drill Down from Components to Additional Data

StdCurCompFind event