WinStudio
Use the Lock Position property to disable changes to the size and position of a component on a form.
Locking is designed to facilitate development of international, multi-language applications. Once a component, such as a static box, has been sized and positioned to accommodate a translated string, you can lock the component to discourage others from repositioning it after applying standard dimensions on it.
Setting | Description |
---|---|
True | Disable changes to the size and position of a component.
If you use this option, all of the Glue... properties are disabled. |
False | Default. Enable changes to the size and position coordinates of a component. |
TIP: You can set the Lock Size property to prevent changes to the just the size of a component without locking its position.
Lock the Size or Position of a Component