WinStudio
Use the Read-Only/Disable property to specify that a component's value cannot be changed by the user or to specify that an unbound component is disabled.
Setting | Description |
---|---|
True | The user cannot change the value of a component bound to a
read-write IDO property. A button or other unbound component is disabled. |
False | Default. The user can change the value of a component bound
to a read-write IDO property. A button or other unbound component is enabled. |
A component bound to a read-only IDO property is automatically read-only, regardless of the value of the Read-Only/Disable property.
Components bound to key IDO properties are enabled for new objects in a collection and are disabled for existing objects. This functionality prevents the user from modifying a key field once an object has been created.
Dynamic enabling/disabling of components is supported by several properties: