WinStudio
The file name of an icon to be displayed in the upper left corner of a form's title bar. The icon overrides the default icon supplied by WinStudio.
On the Form properties sheet, you can select an icon located in the main program folder (the folder in which WinStudio.exe is located) or browse other folders. To locate a file in the main program folder, click the Icon row, click the down pointer, and select a file name. To browse other folders, click the Icon row, then click the ellipsis (...) button.
NOTE: It is recommended that you specify a file located in the main program folder and distribute the file to users in that folder. If you specify a path as well as a file name, the path must be valid on every WinStudio client.