WinStudio
Use the Initial Command property to specify a command that controls what happens when the form opens. These commands are available:
| Setting | Description |
|---|---|
| Refresh | Perform Actions > Refresh.
This option opens the form and immediately returns all records in the collection (up to the record cap). |
| Filter | Perform Actions > Filter by query.
This option opens the form and then immediately opens the query form associated with the form, if one exists. |
| Filter-in-place | Perform Actions > Filter in place.
This option opens the form in Filter-in-Place mode. |
| Add | Perform Actions > New.
This option opens the form in such a way that you are set to create a new record. |
| Event eventname | Execute the specified event. After you select Event from the list, type the event name. |
This property provides a simpler user interface to the underlying mechanism, the form variable InitialCommand.