WinStudio
Use the Parameters property to set specifications for an event handler or validator. For event handlers and validators of the type Inline Script, click the row Edit InLine Script, and then click the ellipsis button to open the script editor. For other types, click the Parameters ellipsis button to set the parameters. Specifications are redisplayed in the Parameters field as a string of WinStudio keywords and their parameters.