WinStudio
IWSApplication interface
Returns or sets an integer value that indicates the maximum number of records to be retrieved when querying a collection.
Application.CollectionCap
Application.CollectionCap = integer
A value of 0 indicates that there is no limit to the number of records that can be retrieved. A value of -1 indicates that the system default collection cap is to be used.
TIP: You can confirm the return value or that the value has been correctly set using the Settings window (View menu > Settings > Runtime tab).
The following example displays a message box that tells what the current collection cap is.
Sub Main()
Dim colCap As String
colCap = Application.CollectionCap.ToString()
Application.ShowMessage("The current collection cap is " & colCap & ".")
End Sub
The following example shows how to use this property to set the collection cap programmatically.
Sub Main() Application.CollectionCap = 75 End Sub