WinStudio
IWSFormComponent interface
Sets or returns a number indicating the greatest number of data (numerals or characters) that a component can have.
integerVar = object.DataLength
Part |
Description |
integerVar | Required. A variable of type integer to hold the return value. |
object | Required. A reference to a form component object. |
object.DataLength = integer
Part |
Description |
object | Required. A reference to a form component object. |
integer | Required. An integer (or variable containing an integer value) that indicates the maximum number of data characters that the component can contain. |
For the Get syntax, the return value is an integer that indicates the maximum number of characters that the designated component can have.
For a list and description of the data types available, see Underlying Type Property.
Sub Main() Dim oComponent As Integer oComponent = ThisForm.Components("LanguageDescGridCol").DataLength Application.ShowMessage("The Description field can have as many as " _ & oComponent.ToString() & " characters.") End Sub
Sub Main() ThisForm.Components("StringTableNameGridCol").DataLength = 10 End Sub