WinStudio
IWSApplication interface
Returns or sets an integer that indicates the maximum number of items to be retrieved and displayed in a drop-down list.
Application.DropDownCap
Application.DropDownCap = integer
A return value of 0 indicates that there is no limit to the number of items that can be retrieved. A value of -1 indicates that the system default drop-down list cap is to be used.
TIP: You can confirm the return value or that the value has been correctly set using the Settings window (View menu > Settings > Runtime tab).
The following example displays a message box that tells what the current collection cap is.
Sub Main()
Dim dropCap As String
dropCap = Application.DropDownCap.ToString()
Application.ShowMessage("The current drop-down list cap is " & dropCap & ".")
End Sub
The following example shows how to use this property to set the collection cap programmatically.
Sub Main() Application.DropDownCap = 100 End Sub