WinStudio
IWSApplication interface
Pads a numeric or alphanumeric string with spaces or zeroes.
Application.ExpandNumSortedChar( string, integer )
Part |
Description |
| string | Required. The original string before it has been padded. |
| integer | Required. The length the string is to be when it has been padded. |
This method appends spaces to the left of a string of numerals. With the string 23 and a length parameter of 5, the method returns " 23".
The method inserts zeroes between the alphabetic and numeric parts of a string of the type abc999. With the string D23 and a length parameter of 5, the method returns D0023.
Strings expanded in this way can be sorted like numbers.
Sub Main
Dim Length As Integer
Dim CustNum As String
Dim CustSeq As String
CustNum = ThisForm.Variables("CustNumV").Value
CustSeq = ThisForm.Variables("CustSeqV").Value
' Ensure CustNum is properly expanded
If ThisForm.PrimaryIDOCollection.IsPropertyNumSortedChar("CustNum") Then
Length = ThisForm.PrimaryIDOCollection.GetPropertyLength("CustNum")
If (Length > 0 And CustNum <> "") Then
CustNum = Application.ExpandNumSortedChar(CustNum, Length)
End If
End If
End Sub