WinStudio

ExportCollection Method

Applies To

IWSIDOCollection interface

Definition

Exports the contents of a designated IDO collection to a file.

Parallels the Form menu option Export to File.

Syntax

object.ExportCollection( Boolean1, string, Boolean2 )

  Part

  Description

object Required. A reference to an IDO collection.
Boolean1 Required. Boolean value that indicates:
  • True means that the output is to be tab-delimited.
  • False means that the output is to be comma-delimited.
string Required. The path and name of the output file.

If you do not specify a full path, the path is relative to the file in which WinStudio.exe is installed.

This method does not create directories.

Boolean2 Required. Boolean value that indicates:
  • True means that the system ignores any record cap and returns all records in the collection. This effectively overrides (for this action) the record set by the system or the user.
  • False means that the system returns only the number of records specified by the record cap in effect on the user's system.

Example

Sub Main()
    ThisForm.PrimaryIDOCollection.ExportCollection(False, "c:\mytemp\Export.csv", False)
End Sub