WinStudio
IWSIDOCollection interface
Retrieves a binary large object (BLOB), such as a graphic image, from an object in a specified row of a collection and writes it to a file.
object.ExportObjectPropertyAsBlob( string1, integer, string2 )
Part |
Description |
object | Required. An expression that evaluates to the name of an IDO collection object. |
string1 | Required. The name of a binary property in the collection. |
integer | Required. Indicates the row in which the specified
object exists.
The row number is zero-based. So, for example, if you want to export the BLOB data from the third row, you must use 2 for this integer |
string2 | Required. The name of the file to which the BLOB
is to be written.
This string must include a path. The path can be relative to the directory containing WinStudio.exe. |
The difference between this method and the ExportCurrentObjectPropertyAsBlob method is that this method acts on an object in a specified (usually other) row, and ExportCurrentObjectPropertyAsBlob references the currently active object.
This method does not create directories.
Sub Main() Dim PropertyName As String Dim FileName As String PropertyName = "blob_column" FileName = "C:\Temp\appGraphics\filter.png" ThisForm.PrimaryIDOCollection.ImportObjectPropertyAsBlob(PropertyName, 4, FileName) FileName = "C:\Temp\ExportBlob.png" ThisForm.PrimaryIDOCollection.ExportObjectPropertyAsBlob(PropertyName, 4, FileName) End Sub
ExportCurrentObjectPropertyAsBlob Method