WinStudio
IWSFormComponent interface
Gets the current date range (All Dates, YTD, PTD, etc) of the Gauge for a Critical Number bound Gauge that is bound to a date driven number.
object.GaugeGetDateRange
| Part | Description |
| object | Required. A reference to a valid gauge component object. |
The return value is a string representing a date range over which the critical number is calculated. Date ranges are supported on IDO based critical numbers that have a date property filled in.
Sub Main()
Application.ShowMessage(ThisForm.Components("gauge1").GaugeGetDateRange)
End Sub