WinStudio
IWSApplication interface
Returns a font descriptor string that indicates the base font used by the application user interface.
A "font descriptor" is a string consisting of a list of fourteen comma-separated values. For details on the font descriptor, see the "Remarks" section.
Application.GetBaseFontDescriptor( )
The return value is a string consisting of a list of fourteen comma-separated values that define the font, using the following format:
Size,0,0,0,Weight,Italic,Underline,Strikethrough,0,0,0,0,0,FontFamilywhere:
List item: |
Consists of: |
| Size | A decimal value representing the point size. |
| Weight | Range from 0 (non-bold) to 700 (bold). |
| Italic | 0 = Normal text. 1 = Italicized text. |
| Underline | 0 = Text not
underlined. 1 = Text underlined. |
| Strikethrough | 0 = Normal text. 1 = Text struck through. |
| FontFamily | Name of the font (family) to be used. |
Sub Main()
Dim FontDesc As String
Dim newFont As Font
FontDesc = Application.GetBaseFontDescriptor()
newFont = Application.FontFromFontDescriptor( FontDesc )
If not IDONull.IsNull(newFont) Then
newFont = new Font( newFont, FontStyle.Bold )
FontDesc = Application.FontDescriptorFromFont( Font.newFont )
End If
ThisForm.Components("FormCollectionGrid").SetGridRowColFont( 3, 4, FontDesc, True )
End Sub