WinStudio
IWSIDOCollection interface
Returns the collection name, which is displayed as the Actions menu name in the WinStudio menu bar.
object.GetDisplayedObjectName
Part |
Description |
object | Required. The name of a valid IDO collection object. |
The return value is a string containing the collection name of the IDO collection object. A collection name is assigned by the developer as part of the collection specification.
If a collection name is not specified for a primary collection, the return value is primary collection. Similarly, the default return value for a subcollection is subcollection for <IDO name> and for a secondary collection, secondary collection n, where n is the number of the collection.
Sub Main() ' Display name associated with the primary IDO collection. Application.ShowMessage(ThisForm.PrimaryIDOCollection.GetDisplayedObjectName()) ' Display name associated with a secondary collection IDO collection. ThisForm.SetFocus("grid1") Application.ShowMessage(ThisForm.CurrentIDOCollection.GetDisplayedObjectName()) End Sub