WinStudio
IWSIDOCollection interface
Returns a string containing the internal value of an object property in the specified IDO collection.
object.GetObjectPropertyInternal( string, integer )
Part |
Description |
object | Required. The name of a valid IDO collection object. |
string | Required. The name of the object property. |
integer | Required. An integer indicating the index number of an object in the specified IDO collection. |
The return value is a string containing the internal value of the object property.
Sub Main() Dim SubColCache As IWSIDOCollection Dim ColCache As IWSIDOCollection Dim NewEntityCode As String Dim i As Integer SubColCache = ThisForm.Components(GetParameter(1)).IDOCollection ColCache = ThisForm.Components(GetParameter(0)).IDOCollection If ColCache.IsCurrentObjectModified Then For i = 0 To SubColCache.GetNumEntries - 1 If SubColCache.IsObjectNew(i) Then ' Loop through the cache entries and, if the row is a new row, place ' the EntityCode value in that row into NewEntityCode NewEntityCode = SubColCache.GetObjectPropertyInternal("EntityCode", i) End If Next i End If End Sub