WinStudio

GraphLockGraphObjects Method

Note: This topic applies to the graphing tool, which is supported for backward compatibility.  We recommend that, if you want to add charts or gauges to a form, use the newer FusionCharts tool instead. For more information, see Adding Charts or Gauges to a Form.

Applies To

IWSFormComponent interface, graph objects

Definition

Locks or unlocks graph objects during run time.

Syntax

object.GraphLockGraphObjects( Boolean )

  Part

  Description

object Required. A reference to a valid graph component object.
Boolean Required. Determines whether graph objects are locked during run time.
  • TRUE - Graph objects are locked.
  • FALSE - Graph objects are unlocked.

Example

ThisForm.Components("graph1").GraphLockGraphObjects( True )