WinStudio
Note: This topic applies to the graphing tool, which is supported for backward compatibility. We recommend that, if you want to add charts or gauges to a form, use the newer FusionCharts tool instead. For more information, see Adding Charts or Gauges to a Form.
IWSFormComponent interface, graph objects
Redraws the graph component with the next set of collection values, according to the number of X-axis limits defined on the component.
object.GraphNext( )
Part |
Description |
object | Required. A reference to a valid graph component object. |
ThisForm.Components("graph1").GraphNext()