WinStudio

GraphPrevious Method

Note: This topic applies to the graphing tool, which is supported for backward compatibility.  We recommend that, if you want to add charts or gauges to a form, use the newer FusionCharts tool instead. For more information, see Adding Charts or Gauges to a Form.

Applies To

IWSFormComponent interface, graph objects

Definition

Redraws the graph component with the previous set of collection values, according to the number of X-axis limits defined on the component.

Syntax

object.GraphPrevious( )

  Part

  Description

object Required. A reference to a valid graph component object.

Example

ThisForm.Components("graph1").GraphPrevious()