WinStudio
Note: This topic applies to the graphing tool, which is supported for backward compatibility. We recommend that, if you want to add charts or gauges to a form, use the newer FusionCharts tool instead. For more information, see Adding Charts or Gauges to a Form.
IWSFormComponent interface, graph objects
Sets the color scheme for the data series.
object.GraphSetDataSeriesColors( colorList )
Part |
Description |
| object | Required. A reference to a valid graph component object. |
| colorList | Required. Of the class System.Collections.Generic.List(Of String). |
Colors are defined in RGB (Red,Green,Blue) string format. The system accepts numbers in the range 0–255 for each RGB value.
If an invalid RGB string value is given, the system ignores the color specification.
The system interprets an empty string as an RGB value of 0,0,0.
Dim seriesColors As System.Collections.Generic.List(Of String) = _
New System.Collections.Generic.List(Of String)
seriesColors.Add("255,0,0") ' Red
seriesColors.Add("255,255,0") ' Yellow
seriesColors.Add("0,0,255") ' Blue
ThisForm.Components("graph1").GraphSetDataSeriesColors( seriesColors )
ThisForm.Components("graph1").GraphDraw()