WinStudio

GraphSetMainTitleFontDescriptor Method

Note: This topic applies to the graphing tool, which is supported for backward compatibility.  We recommend that, if you want to add charts or gauges to a form, use the newer FusionCharts tool instead. For more information, see Adding Charts or Gauges to a Form.

Applies To

IWSFormComponent interface, graph objects

Definition

Sets the font for the graph's main title.

Syntax

object.GraphSetMainTitleFontDescriptor( string )

  Part

  Description

object Required. A reference to a valid graph component object.
string Required. Consists of fourteen comma-separated values:

    Size,0,0,0,Weight,Italic,Underline,Strikethrough,0,0,0,0,0,FontFamily

For more information about these values, see the "Settings" section.

Settings

  Setting

  Description

Size A decimal value representing the point size.
Weight Range from 0 (non-bold) to 700 (bold).
Italic 0 = Normal text.
1 = Italicized text.
Underline 0 = Text not underlined.
1 = Text underlined.
Strikethrough 0 = Normal text.
1 = Text struck through.
FontFamily Name of the font to be used.

Example

Dim fontDescriptor As String = "16,0,0,0,700,0,0,0,0,0,0,0,0,Arial"   ' 16-point bold Arial
ThisForm.Components("graph1").GraphSetMainTitleFontDescriptor(fontDescriptor) 
ThisForm.Components("graph1").GraphDraw()