WinStudio
Note: This topic applies to the graphing tool, which is supported for backward compatibility. We recommend that, if you want to add charts or gauges to a form, use the newer FusionCharts tool instead. For more information, see Adding Charts or Gauges to a Form.
IWSFormComponent interface, graph objects
Sets the font for other titles found in the graph (titles found on the x- and y-axes).
object.GraphSetMainTitleFontDescriptor( string )
Part |
Description |
object | Required. A reference to a valid graph component object. |
string | Required. Consists of fourteen comma-separated
values:
Size,0,0,0,Weight,Italic,Underline,Strikethrough,0,0,0,0,0,FontFamily For more information about these values, see the "Settings" section. |
Setting |
Description |
Size | A decimal value representing the point size. |
Weight | Range from 0 (non-bold) to 700 (bold). |
Italic | 0 = Normal text. 1 = Italicized text. |
Underline | 0 = Text not
underlined. 1 = Text underlined. |
Strikethrough | 0 = Normal text. 1 = Text struck through. |
FontFamily | Name of the font to be used. |
Dim fontDescriptor As String = _ "12,0,0,0,700,0,0,0,0,0,0,0,0,Times New Roman" ' 12-point bold Times New Roman ThisForm.Components("graph1").GraphSetMainTitleFontDescriptor(fontDescriptor) ThisForm.Components("graph1").GraphDraw()