WinStudio
Note: This topic applies to the graphing tool, which is supported for backward compatibility. We recommend that, if you want to add charts or gauges to a form, use the newer FusionCharts tool instead. For more information, see Adding Charts or Gauges to a Form.
IWSFormComponent interface, graph objects
Sets the number of data points (number of IDO collection rows) on the x-axis.
object.GraphSetXLimit( integer )
Part |
Description |
object | Required. A reference to a valid graph component object. |
integer | Required. The number of data points to be represented and displayed at one time. |
ThisForm.Components("graph1").GraphSetXLimit(8) ThisForm.Components("graph1").GraphDraw()