WinStudio
IWSIDOCollection interface
Imports a binary large object (BLOB), such as a graphic image, from a file and loads it in a specified property of a collection.
object.ImportBlob (PropertyName, RowNumber, FileName)
Part |
Description |
object | Required. An expression that evaluates to the name of an IDO collection object. |
PropertyName | Required. The name of a Binary property in the collection. |
RowNumber | Required. An integer indicating the row into which the property is to be imported. |
FileName | Required. The name of the file containing the BLOB. FileName must include the path. The path can be relative to the directory containing WinStudio.exe. |
The difference between this method and the ImportCurrentObjectPropertyAsBlob method is that this one imports to an object in a specified (other) row, and ImportCurrentObjectPropertyAsBlob imports the BLOB to the currently active object.
This example imports a bitmap from a file named Splash.BMP into a property named Photo in the fourth row of a collection and then exports it from that row to a temporary file named Splash_VBA_TEST.BMP.
Sub Main() Dim PropertyName As String Dim FileName As String PropertyName = "Photo" FileName = ".\res\Splash.BMP" ThisForm.PrimaryIDOCollection.ImportObjectPropertyAsBlob( PropertyName, 4, FileName ) FileName = "C:\Temp\Splash_VBA_TEST.BMP" ThisForm.PrimaryIDOCollection.ExportObjectPropertyAsBlob( PropertyName, 4, FileName ) End Sub