WinStudio
IWSIDOCollection interface
Returns a Boolean value indicating whether the current object is the first (or top) entry in the specified IDO collection.
object.IsBOF( )
Part |
Description |
| object | Required. The name of a valid IDO collection object. |
A return value of:
Sub Main()
Dim bIsLast As Boolean
Dim bIsFirst As Boolean
bIsFirst = ThisForm.CurrentIDOCollection.IsBOF()
bIsLast = ThisForm.CurrentIDOCollection.IsEOF()
If bIsLast = True Then
Application.ShowMessage("The selected object is the last item.")
ElseIf bIsFirst = True Then
Application.ShowMessage("The selected object is the first item.")
Else
Application.ShowMessage("The selected object is not first or last.")
End If
End Sub