WinStudio

IsCurrentObjectDeleted Method

Applies To

IWSIDOCollection interface

Definition

Returns a Boolean value indicating whether the current object in the specified IDO collection is marked for deletion.

Syntax

object.IsCurrentObjectDeleted( )

  Part

  Description

object Required. The name of a valid IDO collection object.

Remarks

A return value of:

If the specified IDO collection has the focus, use this method. If the specified collection might not have the focus, use the IsObjectDeleted method.

Example

Sub Main()
   If ThisForm.PrimaryIDOCollection.IsCurrentObjectDeleted() Then
      ThisForm.Components("comboBox1").Enabled() = False
   Else
      ThisForm.Components("comboBox1").Enabled() = True
   End If
End Sub